Power

Power Solutions and Technologies

Contents

Top

Discrete Power Components

Silicon (Si), Silicon Carbide (SiC), and Gallium Nitride (GaN) Semiconductors

Gate Drivers​

Transistors

Diodes

Thyristors

Power Management Integrated Circuits (PMICs)

Linear Voltage Regulators

Switching Voltage Regulators

Power Supplies

Isolated Power Supply

Non-Isolated Power Supply

Limits on Isolated Power Supplies

What form factors do power supplies come in?

Off-Board Power Supplies

Board Mount Power Supplies

Power Bricks

Thermal Management in Power

Fans

Heat Sinks

Thermal Interface Materials (TIM)

Products

Power Solutions and Technologies

Primary power electronics topologies:​

There are three main categories of power electronics products at DigiKey:

  • Discrete Power Components: Referring to components that can be used with PMICs, or individually to create specifically tailored solutions. Getting down to this level provides the greatest flexibility but also commonly the greatest amount of development and expertise is required.
  • Power Management Integrated Circuit (PMIC): Referring to a wide range of Application-Specific ICs or ASICs. They generally take more planning (and often additional discrete components) to create a full solution than using a power supply.
  • Power Supplies: Referring to a device which transforms power, often stepping up or down a voltage. There is not as much customization at this level and leaves the power solution to more of a black box.

There's also an overarching theme of Thermal Management.

 

For further reading on some of the cutting edge power technologies and applications, be sure to read the power issue of the Digi-Key eMagazine, available here.​

The 2024 Power issue of the Digikey eMagazine.

Discrete Power Components

Discrete power components are the individual devices that can be put together to play the same role as a PMIC or power supply. Semiconductor discrete components for power include transistors, diodes, and thyristors. Whereas passive components for power include resistors, capacitors, and inductors.

Silicon (Si), Silicon Carbide (SiC), and Gallium Nitride (GaN) Semiconductors

Frequency and power ranges best suited for Differing Semicondutor material devices
Photo Credit: GaN: Pushing the limits of power density & efficiency

Traditional Semiconductor:

  • Silicon (Si) – Traditional silicon-based semiconductor devices were the first generation of integrated circuit devices and are among the most common type of ICs found on the market day. Silicon typically has a lower cost per unit and is a more researched semiconductor element.

Image of onsemi logo

Image of onsemi NTBLS1D5N10MC Power MOSFET

onsemi’s NTBLS1D5N10MC single, N-channel power MOSFET powers up applications efficiently and with minimal energy loss.

Image of Infineon Technology Logo

Image of Infineon's 650 V and 1200 V TRENCHSTOP™ IGBT7 H7

Infineon Technologies advanced TRENCHSTOP™ IGBT7 H7 technology addresses the rising demand for green and efficient energy applications.

Wide Band Gap (WBG) Semiconductors:

  • Silicon Carbide (SiC) – SiC is a wide bandgap semiconductor material made up of silicon (Si) and carbon (C). Carbon is a hard and durable material found in high performance brake pads and grinding wheels can also be found high voltage power applications where its breakdown voltage is 10 times higher when compared to traditional Silicon based parts. SiC based components can typically handle higher operating voltages, higher temperatures, and typically require a smaller footprint.

Image of Infineon Technology Logo

Image of Infineon Technologies CoolSiC™ G2 1200 V Silicon Carbide MOSFET Discretes

Infineon CoolSiC™ G2 silicon carbide (SiC) MOSFET discretes allow for the lowest application losses and the highest operational reliability.

Image of Microchip color logo

Image of Microchip's MSC400SMA330 3300V Silicon Carbide (SiC) MOSFET

Microchip's MSC400SMA330, 3300 V silicon carbide (SiC) MOSFET ensures no performance degradation over the life of the end equipment.

  • Gallium Nitride (GaN) – GaN is composed of Gallium (Ga) and Nitrogen (N). GaN is a wide bandgap semiconductor material, offering even better switching speed, power handling and thermal dissipation compared to SiC and Si. Found in applications that require high power and high switching frequencies, GaN based components are rapidly becoming a favorite component for engineers looking for high efficiency, low power loss and compact form factor.

Image of ROHM Semiconductor logo

Image of ROHM’s 650 V GaN HEMTs

ROHM's 650 V GaN HEMTs increase efficiency and miniaturization in a wide range of power supply systems, including servers and AC adapters.

Image of EPC Logo

Image of EPC's EPC2218A and EPC2204A GaN FETs

EPC's EPC2218A and EPC2204A GaN FETs offer state-of-the-art power density.

Image of Related Content Card: Why and How to Apply GaN Field Effect Transistors

Improve power efficiency and power density in higher voltage switch-mode power systems by understanding the principles and correct application of GaN FETs.

Bővebben

Image of Related Content Card: Wide Bandgap Semiconductors Are Reshaping the Transportation World

The entire transportation sector is undergoing a radical transformation with solutions for electric and hybrid cars and cleaner mass transportation.

Bővebben

Image of Related Content Card: Wide Bandgap Semiconductors Drive Efficiency in Datacenters

Since datacenters have huge energy requirements, power solutions that can reduce power losses, boost efficiency, and enhance thermal control are required.

Bővebben

Gate Drivers​

A gate driver is a type of power amplifier circuit that takes a low power input signal, such as a from a microcontroller, and produces a high-power output signal to drive a gate terminal for high-power transistors such as a power MOSFET or Insulated-Gate Bipolar Transistor (IGBT).​

​Gate drivers are an important bridge linking the low power logic side and the high-power driving circuity of many applications like power conversion and motor control.​

​Gate drivers can also provide other protection features such as electrical isolation, voltage level shifting, and signal conditioning.​

What does a gate driver do? View Answer

Gate drivers provide a high current output signal that can rapidly charge or discharge a gate terminal on a power transistor like a MOSFET or IGBT.​

High frequency switch mode power supplies (SMPS) or Brushless DC (BLDC) motors require low voltage logic levels (like those from microcontrollers) to quickly charge / discharge. The gate driver amplifies the low voltage logic levels to operate the larger power transistors at these faster frequencies.​

Image of Infineon Technology Logo

1ED38xx EiceDRIVER™ Isolated Gate Driver family - Infineon

Infineon's EiceDRIVER™ Enhanced 1ED38xx (X3 digital) is a family of 5.7 kV single-channel highly flexible isolated gate drivers.

Image of onsemi logo

Image of onsemi's NCD57090 Isolated High Current Gate Driver

onsemi's NCD57090 isolated high-current gate driver is designed for high system efficiency and reliability in high-power applications.

The high-side/low-side arrangement of a gate driver

The driver is the interface component or “bridge” between the low-voltage, low-current output of the system processor operating in a controlled, benign scenario and the rough-and-tumble world of the switching device with its strict requirements on current, voltage, and timing.

Bővebben

Screen capture of the webinar

Every silicon carbide switch requires a gate driver. This webinar from Industry Tech Days 2023 provides an easy-to-use matrix for selecting the correct gate driver for your silicon carbide applications.

Bővebben

A detail of a circuit schematic for a gate driver circuit

The most critical moments in the gate drive are the turn-on and turn-off of the IGBT. The goal is to perform this function quickly, but with minimal noise and ringing when the IGBT is turned on.

Bővebben

Transistors

Discrete semiconductor devices that amplify or switch power signals. Transistors are typically three terminal devices.

Transistors Product Selection Guide

  • FETs, MOSFETs – Field-Effect Transistor (FET) is a transistor that operates off field-effect to control current flowing through the drain and source. Metal-Oxide Semiconductor Field-Effect Transistor (MOSFET) is a four terminal FET that is widely used in switched mode power supplies.
  • IGBTs – Insulated Gate Bipolar Transistors (IGBTs) are four-layer semiconductor devices (PNPN) that can handle high currents and used mainly for switching.
  • HEMTs – High-electron-mobility transistor (HEMT) is a FET that incorporates different band gap materials.

Diodes

Diodes are usually semiconductors, there goal being to allow current in only one direction.

Image of Related Content Card: Diodes - TechForum

The term “diode” is applied to a large number of two-terminal devices with varied functions.

Bővebben

Image of Related Content Card: Schottky vs Standard Diode

Diodes come in several different shapes and flavors, from tiny glass encapsulated Zener diodes to incredibly large rectifier diode PUK modules. Schottky diodes fall into this spectrum somewhere in the middle of things.

Bővebben

  • Rectifier Diode – Used often to convert an AC wave form into a unipolar waveform. A single rectifier diode maybe used in a half-wave rectifier, where as a bridge rectifier can be used in full-wave rectification.
  • Zener Diode – Zener diodes are created to gracefully operate in a forward and reverse current direction. The reverse direction of current is enabled when Zener voltage is reached.

Thyristors

Thyristors are four-layer semiconductor devices (PNPN) that act as a switch that only let current flow when a pulse is applied to its gate.

Image of Related Content Card: Thyristors - SCRs

This Product Selection Guide contains information to help select products in the Thyristors - SCRs category on DigiKey.com

Bővebben

Image of Related Content Card: Thyristors - DIACs, SIDACs

This Product Selection Guide contains information to help select products in the Discrete Semiconductors - Thyristors - DIACs, SIDACs category on DigiKey.com

Bővebben

Image of Related Content Card: Thyristors - TRIACs

This Product Selection Guide contains information to help select products in the Thyristors - TRIACs category on DigiKey.com

Bővebben

Power Management Integrated Circuits (PMICs)

PMIC, or Power Management Integrated Circuits, refer to a wide range of Application-Specific ICs or ASICs. These devices are intended to be either be bread boarded in a prototyping phase or soldered to a PCB in a production phase. They generally take more planning (and often additional discrete components) to create a full solution than using a power supply.

What is the difference between linear and switching regulators? View Answer

Linear and Switching Regulators are DC-DC Converters that get commonly used to stabilize output voltage supplied to the load.

Linear Regulators are often a starting point for a school project, as they are generally cheaper and easier to use. Linear Regulators create a constant output voltage by using a series of transistors, and the excess voltage gets dissipated as heat. The downside is that the dissipated heat is wasted energy, and if there's too much heat dissipated in this way, it can destroy the regulator.

Switching Voltage regulators can more efficiently stabilize the voltage output and waste less energy in the process. Switching Voltage regulators can be a good investment if you have a project that is consistently powered, or if you're looking for something more robust.

Linear Voltage Regulators

Linear Voltage Regulators are DC-DC Converters that can output a stable output voltage. Linear Voltage Regulators need to account for the power loss it can introduce and the resulting heat dissipation. It can be advantageous over a switching regulator in some cases due to its small footprint, high accuracy, and low output noise. Generally, more suitable for low current applications due to efficiency and power dissipation concerns.​

  • Low Dropout (LDO) Linear Regulator - can have the input voltage close to the output voltage which reduces the amount of power loss.​
An example of an LDO​
Source: Texas Instruments

Switching Voltage Regulators

Switching voltage regulators take the input signal and quickly turn it on and off to create a stable output voltage. There is generally less power loss in a switching regulator. Also, there are a wider range of input to output voltages that can be covered by a switching regulator.

Some Common Types of DC-DC Switching Regulators

  • Buck - A buck converter circuit is used to decrease the output voltage and can increase the output current. The Buck converter circuits uses inductors, capacitors, and 'switches'. The 'switches' are typically a semiconductor MOSFET. This circuit topology is commonly found in electronic devices that require a low voltage to supply components off a higher system voltage supply.​
Simplified Schematic of a Buck Converter Power Stage
Source: Texas Instruments​
  • Boost - A boost converter circuit is used to increase the output voltage. A boost converter uses inductors, capacitors, and 'switches'. The 'switches' are typically a semiconductor MOSFET. Boost converters are typically found in applications that require a higher operating voltage then the supply voltage such as lighting drivers or portable power supplies.
Simplified Schematic of a Boost Converter Power Stage
Source: Texas Instruments​
  • Buck Boost - A Buck Boost converter circuit can have an output voltage either higher or lower than the input voltage. As the name suggest a Buck Boost converter uses circuit features found in both Buck and Boost converters.
Simplified Schematic of an Inverting Buck-Boost Stage
Source: Texas Instruments​
Image of Related Content Card: Reference Design Library – AC/DC and DC/DC Conversion

AC/DC and DC/DC Conversion reference designs including schematics, specifications, and support documents available in Digi-Key’s Reference Design Library.

Bővebben

Screen Capture of a Buck Converter schematic from a video

Have you ever wondered how switch mode power supplies work? Buck converters regulate input voltages down to lower output voltages in a very efficient way.

Bővebben

Image of Related Content Card: Linear Voltage Regulator vs. Switching Regulator

When designing a powered device, the question sometimes arises of whether a Linear Voltage Regulator or a Switching Regulator is more suitable for the design.

Bővebben

Image of Related Content Card: Reference Design Library – Power Management

Power Management reference designs including schematics, specifications, and support documents available in Digi-Key’s Reference Design Library.

Bővebben

Image of Related Content Card: Another Teaching Moment - What is a Voltage Regulator

Selection of the right type of voltage regulator is critical in the world of effective electronic circuit design.

Bővebben

Power Supplies

Power Supplies in this context are used to describe a self-contained device that takes electrical power from a source and converts it to a suitable load power.

Power Supply Diagram

What is the difference between isolated and non-isolated power supplies? View Answer

Galvanic isolation means that there are separate electrical and physical paths between the input and output circuits. This electrical isolation is commonly achieved via a transformer or coupled inductors between the input and output circuitry. AC-DC conversion is usually isolated, and isolation becomes more of a variable in DC-DC conversion. The reasons for creating the isolation is usually for safety (reducing the chance of shock to anyone operating near the power supply), or reduction of noise to the output circuit.

Isolated Power Supply

Non-Isolated Power Supply

Limits on Isolated Power Supplies

The isolation voltage (on the data-sheet) is the short-term amount of voltage that can be experienced without breakdown. Working voltage or maximum operating voltage is the continuous maximum voltage that can be applied without breakdown.

Image of Related Content Card: Power Module in Isolated DC/DC Bias Power Supplies

Power modules have a wide range of uses and have significant integration compared to discrete implementations.

Bővebben

Image of Introduction to DC-DC Converters

DC-DC converters are widely used to efficiently produce a regulated voltage from a source that may or may not be well controlled to a load that may or may not be constant.

Bővebben

What form factors do power supplies come in?

Board mount power supplies are products that are intended to be directly affixed to a Printed Circuit Board (PCB), whereas off-board power supplies are not.

What is the difference between off-board and board mount power supplies? View Answer

Board mount power supplies are products that are integrated directly into the system they power. They are directly affixed to a Printed Circuit Board (PCB). Off-board power supplies are sometimes referred to as external power supplies. An example of an off-board power supply is a wall mount plug. The adapter plugs into the wall and then interfaces to the system via a connector.

Off-Board Power Supplies

Enclosed vs Open Frame

Enclosed – The enclosure gives a layer of protection from debris, it increases safety, however this enclosure is likely to trap heat and often requires more cooling.
Open Frame – Open frame does not come with a lid. It runs an increased risk of shock or electrocution (due to exposed components). Open frame supplies generally run a smaller footprint than enclosed power supplies.

Connectors / Plug types for wall adapters

Barrel Connector – commonly used with a wall mounted AC-DC converter for items like laptop computers and printers
IEC 320-C14 – commonly used with computer monitors or self-power speakers
IEC 320-C8 (figure-8) – commonly used in office equipment and printers
NEMA 1-15P (Type A) – common outlet type found in the United States
CEE 7/16 or Type C (Europlug) – common outlet found in Europe
Universal Serial Bus (USB) – commonly found on computers
A world map focused on the Northern Hemisphere with the Continental United States highlighted

DigiKey's Electrical Plug Reference Calculator is a tool designed to assist users in determining the compatibility of electrical plugs and outlets in different regions and countries.

Bővebben

Image of Related Content Card: Around the World with Power Plugs

The world has never had a standard style of power plug and probably never will. The history of how types of plugs came to be is varied and colorful.

Bővebben

Image of Related Content Card: Finding a Replacement Power Supply

One very common question we receive here at Digi-Key is customers looking for replacement power supplies. The majority of these are AC to DC adapters and can be found in our AC DC Desktop, Wall Adapters Section.

Bővebben

Image of Related Content Card: Using a Switching Power Supply for Battery Charging

Constant current charging is a way to charge common batteries. This is a charging method where batteries are charged with a constant current from beginning to end.

Bővebben

Board Mount Power Supplies

Board mount power supplies, are intended to be affixed to a Printed Circuit Board (PCB).

Power Bricks

Learn more about power supply bricks

Thermal Management in Power

Any machine, circuit, switching device, or power converter is less than 100% efficient. This is due to energy loss, which can come from many factors: the slight resistance found in a conductor, switching losses, and even in mechanical vibrations between parts. This energy loss is typically converted into forms that are unable to do useful work: vibrations, sounds, and heat.

As heat from power loss is generated it must be dealt with by the designer or the whole device could experience shorten life span, out of specification performance, or in the worse case it could be a danger to users. Luckily, there are several methods for dealing with waste heat generated by power devices.

Fans

Just like personal fans found in your living space can help keep areas cool by moving air, electronic devices can have fans as well to move air into or out of an enclosure. By either drawing external air into the enclosure or by exhausting heated air from inside, fans allow a large degree of flexibility when designing heat flow and management.

Source: DigiKey
Pros Cons
Small and compact form factors Moving parts - has the likelihood to be the first part in a system to fail
Can specify air flow Can require separate power circuits, and increase cost
Fan speed can be regulated based on a feedback loop Can include more complex feedback loops

Heat Sinks

Heat sinks are a completely passive device that allows for the transfer of heat away from a source into the surrounding environment. Typically, heat sinks are found in direct contact with high power devices such as CPUs, or power bricks that need to be cooled directly.

Source: DigiKey
Pros Cons
No moving parts, and does not break easily Heavy and large
Can be paired with fans to improve heat transfer Effectiveness dependent on surrounding temperature
Variety of shape, size, and package type Calculating effective sizing may require more complex math

Thermal Interface Materials (TIM)

Thermal Interface Materials also known as TIMs, are materials or substance that can be placed between two larger components to improve the thermal transfer between them, such as a power supply and an external heat sink. TIMs are typically either a thin sheet of material or spreadable paste which can be applied or spread over the device to help increase the thermal conductivity between two items.

Source: DigiKey
Pros Cons
For sheets: solid material sheets can be cut to size and shape Can be expensive
For dispensable: able to be spread and apply onto nearly any surface Typically has a shelf life or use by date
Greatly improve thermal conductively by removing air gaps between dissimilar materials Most do not provide mechanical strength or connections without adhesives
Image of Fan-Driven, Forced-Air Cooling

Using fans for cooling electronics is a standard technique, but should they push air in or pull it out of the assembly they are cooling?

Bővebben

Image How to Stay Cool

Carefully select heat sinks to lower component temperature and improve reliability.

Bővebben

Image An Introduction to Thermal Management

As more is demanded of electronic systems, theory dictates three ways heat is transferred thereby cooling components: conduction, convection, and radiation.

Bővebben

Image Don’t Forget About Thermal Interface Materials

A Thermal Interface Material (TIM) is of utmost importance in providing optimal performance for fans, heatsinks, and Peltier devices.

Bővebben

Products

Integrált áramkörök (IC-k)

Fogyasztásszabályozás/energiagazdálkodás (PMIC) 222939 árucikk

Akkumulátorfigyelés 4612 árucikk

Akkumulátortöltők 3353 árucikk

Áramszabályozás 1381 árucikk

Egyenirányítós áramátalakítók, hálózati, kapcsolóüzemű 4394 árucikk

Energiaelosztó kapcsolók, áramellátás-szabályozás 7208 árucikk

Ethernetes áramellátás (PoE) – vezérlőegységek 759 árucikk

Felügyeleti IC-k 37984 árucikk

Feszültség–frekvencia (V/F) és frekvencia–feszültség (F/V) átalakítók 134 árucikk

Feszültségreferencia-adók 8373 árucikk

Feszültségszabályozók – kapcsolóüzemű, egyenáram-átalakítós feszültségszabályozók 36146 árucikk

Feszültségszabályozók – lineáris + kapcsolóüzemű 1467 árucikk

Feszültségszabályozók – lineáris, kis feszültségesésű (LDO) feszültségszabályozók 66744 árucikk

Fogyasztásmérők 457 árucikk

Fogyasztásszabályozás/energiagazdálkodás – különleges célú 7199 árucikk

Hőszabályozás 456 árucikk

Kapuvezérlők 6287 árucikk

Kijelzőmeghajtók 1131 árucikk

Kikapcsolás nélkül cserélhető vezérlőegységek 2009 árucikk

LED-meghajtók 6667 árucikk

Lézermeghajtók 343 árucikk

RMS–egyenáram átalakítók 132 árucikk

Tápegységek – tápegység-vezérlők és -figyelők 1841 árucikk

Teljes hidas és félhidas meghajtók 1317 árucikk

Teljesítménytényező-javítók (PFC-k) 1034 árucikk

VAGY kapuként működő (ORing) vezérlők, ideális diódák 638 árucikk

Világítás – vezérlő előtétek 446 árucikk

Villanymotor-vezérlők 4882 árucikk