Maker.io main logo

GPS Time & Internet Time As a Backup Using Visuino

76

2025-06-04 | By Ron Cutts

License: GNU Lesser General Public License Displays GPS LCD / TFT Real Time Clocks (RTCs) Wifi Arduino ESP8266

In this Visuino project, ensure accurate timekeeping with a dual-source system! The ESP8266-D1 Arduino-compatible board retrieves time from the NEO-6M GPS module. If the GPS signal is lost, the board automatically switches to Wi-Fi and fetches the accurate date and time from an NTP server. This makes it a perfect backup solution for real-time applications!

Watch the video!

Big thanks to Stephan Buth for this great project idea! Check out his Youtube channel!

Step 1: What You Will Need

What You Will Need

What You Will Need

What You Will Need

What You Will Need

What You Will Need

What You Will Need

  1. ESP8266-D1 Arduino Compatible Development Board (Or any other board with WiFi)

  2. NEO-6M GPS Breakout Module with Antenna

  3. Breadboard

  4. LCD I2C 16X2

  5. Jumper wires

  6. Visuino software: Download here

Step 2: The Circuit

The Circuit

  1. Connect LCD pin [SCL] to ESP8266-D1 pin [SCL]

  2. Connect LCD Sensor pin [SDA] to ESP8266-D1 pin [SDA]

  3. Connect LCD Sensor pin [VCC] to ESP8266-D1 pin [5v]

  4. Connect LCD Sensor pin [GND] to ESP8266-D1 pin [GND]

  1. Connect NEO-6M GPS module pin [VCC] to ESP8266-D1 pin [5v]

  2. Connect NEO-6M GPS module pin [GND] to ESP8266-D1 pin [GND]

  3. Connect NEO-6M GPS module pin [TX] to ESP8266-D1 pin [RX]

Step 3: Start Visuino, and Select the WeMos D1 / R2 Board Type

Start Visuino, and Select the WeMos D1 / R2 Board Type

Start Visuino, and Select the WeMos D1 / R2 Board Type

The Visuino: https://www.visuino.com also needs to be installed. Download the free version or register for a free trial.

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "WeMos D1 / R2" as shown in Picture 2

Step 4: WiFi Setup

WiFi Setup

WiFi Setup

WiFi Setup

WiFi Setup

WiFi Setup

WiFi Setup

Select WeMos D1 / R2 board and in the editor Modules>WiFi>Access Points, click the [...] button, so that the "Access points " window will open. In this editor, drag the WiFi access point to the left side.

  1. In the properties window, under "SSID" put the name of your WiFi Network

  2. Under "Password" put the access password for your WiFi network

  3. Close the "Access points" window

  4. On the left in the editor, select Modules>Wifi>Sockets, click the [...] button, so that the "Sockets" window will open. Drag the TCP/IP Client from right to the left side, then under the properties window, set port: 37 and host: time-c-g.nist.gov

  5. Close the "Sockets" window

Step 5: In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

In Visuino Add & Set Components

  1. Add "Liquid Crystal Display (LCD) - I2C" component

  2. Double click on the "LiquidCrystalDisplay1" and in the Elements window, drag "Text Field" to the left side

  3. In the Elements window, drag another "Text Field" to the left side and in the properties window set "Row" to 1, "Initial Value" to ------

  4. Close the Elements window

  1. Add "Serial GPS" component

  2. Add "Digital Multi Source" component, and in the properties window set "Output Pins" to 4

  3. Add "Digital (Boolean) Inverter (Not)" component

  4. Add 2X "Date/Time On/Off Switch" component, and for both in the properties window set "Send On Enable" to True

  5. Add 2X "Detect Edge(Digital to Clock)" component, and for the first one in the properties window, set "On Rising/True" to False

  6. Add "Internet Time Protocol" component

  7. Add "Date/Time Multi-Source Merger" component

  8. Add "Text Value" component

  9. Double click on "TextValue1" and in the Elements window, drag "Set Value" to the left side, and in the properties window, set "Value" to Internet Time

  10. Drag another "Set Value" to the left side, and in the properties window, set "Value" to GPS Time

  11. Close the Elements window

Step 6: In Visuino Connect Components

image

image

Connect "GPS1" pin [Out] to WeMos D1 / R2 Serial [0] pin [In]

  1. Connect "GPS1" pin [Date Time] to "Switch1" pin [In]

  2. Connect "GPS1" pin [Invalid] to "MultiSource1" pin [In]

  3. Connect "MultiSource1" pin [0] to "Inverter1" pin [In]

  4. Connect "MultiSource1" pin [1] to "Switch2" pin [Enable]

  5. Connect "MultiSource1" pin [2] to "DetectEdge1" pin [In]

  6. Connect "MultiSource1" pin [3] to "DetectEdge2" pin [In]

  7. Connect "Inverter1" pin [Out] to "Switch1" pin [Enable]

  8. Connect "Switch1" pin [Out] to "DateTimeMultiMerger1" pin [0]

  9. Connect "Switch2" pin [Out] to "DateTimeMultiMerger1" pin [1]

  10. Connect "DetectEdge1" pin [Out] to "TextValue1" > "Set Value2" pin [In]

  11. Connect "DetectEdge2" pin [Out] to "TextValue1" > "Set Value1" pin [In]

  12. Connect "DetectEdge2" pin [Out] to "InternetTime1" pin [Clock]

  13. Connect "InternetTime1" pin [Out] to "Switch2" pin [In]

  14. Connect "InternetTime1" pin [Socket] to "WeMos D1 / R2" >TCP Client1 pin [In]

  15. Connect "DateTimeMultiMerger1" pin [Out] to "LiquidCrystalDisplay1" > "Text Field2" pin [In]

  16. Connect "TextValue1" pin [Out] to "LiquidCrystalDisplay1" > "Text Field2" pin [In]

  17. Connect "LiquidCrystalDisplay1" pin I2C Control to "WeMos D1 / R2" I2C In

Step 7: Generate, Compile, and Upload the Code

Generate, Compile, and Upload the Code

Before uploading, disconnect the RX pin on the board, and after uploading, connect it back.

In Visuino, at the bottom, click on the "Build" Tab, make sure the correct port is selected, then click the "Compile/Build and Upload" button.

Step 8: Play

If you power the ESP board, the LCD will start to show the GPS Date & Time. If the GPS Signal is lost, it will connect to the Internet time server and get the current Date & Time.

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project for this. You can download it and open it in Visuino: https://www.visuino.com

Download Visuino File: GPS-INT-BACKUP-TIME.visuino

Gyártói cikkszám 26046
ARDUINO AND NODEMCU COMPATIBLE
CANADUINO®
2 456,53 Ft
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.