Intro to Embedded Rust Part 5: Reading from an I2C Temperature Sensor | DigiKey
This tutorial covers how to use Inter-Integrated Circuit (I2C) communication in embedded Rust on the Raspberry Pi Pico 2. I2C is one of the most widely used protocols in embedded systems, enabling microcontrollers to communicate with sensors, displays, memory chips, and countless other peripherals using just two wires. We'll build on our USB serial template to create a temperature monitoring application that reads data from a TMP102 I2C sensor and displays it over USB serial when you press a button. The written guide for this episode can be found here: https://www.digikey.com/en/maker/tutorials/2026/intro-to-embedded-rust-part-5-reading-from-an-i2c-temperature-sensor The GitHub repository containing the Docker image and example code for this series can be found here: https://github.com/ShawnHymel/introduction-to-embedded-rust We’ll explore how to configure GPIO pins for their alternate I2C functions using the rp235x-hal, initialize the I2C peripheral with the proper clock speed (100 kHz standard mode), and perform write-read operations to communicate with I2C devices. We explain I2C addressing and how to access device registers. The tutorial walks through reading the TMP102's datasheet to understand its register layout, performing combined write-read transactions, and converting raw binary sensor data into meaningful temperature values in degrees Celsius. You'll see practical bit manipulation techniques including shifting and masking to extract 12-bit signed temperature values from the sensor's two-byte response. The project also introduces important embedded Rust patterns beyond just I2C. We demonstrate button input handling with pull-up resistors and implementing edge detection to trigger readings only on button press. You'll see how to use the heapless crate to work with fixed-size strings without heap allocation (essential for no-std embedded development where heap usage is often avoided). We show how to format floating-point temperature values into strings using the write! macro and core::fmt::Write trait, providing formatted output without the standard library. The tutorial also covers practical error handling for I2C operations using Rust's Result type, showing how to gracefully handle communication failures and display error messages over USB serial. The demo used in this tutorial provides a reusable template for interfacing with I2C devices that you can adapt for accelerometers, gyroscopes, displays, EEPROMs, and thousands of other I2C peripherals.
Part List
| Kép | Gyártói cikkszám | Leírás | Available Quantity | Ár | Részletek megtekintése | |
|---|---|---|---|---|---|---|
![]() | ![]() | 1957 | JUMPER WIRE M TO M 6" 28AWG | 3907 - Immediate | $624.57 | Részletek megtekintése |
![]() | ![]() | FIT0096 | BREADBRD TERM STRIP 3.20X2.00" | 3713 - Immediate | $928.84 | Részletek megtekintése |
![]() | ![]() | CF14JT220R | RES 220 OHM 5% 1/4W AXIAL | 93369 - Immediate 30000 - Factory Stock | $32.03 | Részletek megtekintése |
![]() | ![]() | 1825910-6 | SWITCH TACTILE SPST-NO 0.05A 24V | 45941 - Immediate | $41.64 | Részletek megtekintése |
![]() | ![]() | DH-20M50055 | USB AM TO USB MICRO, USB 2.0 - 1 | 9354 - Immediate | $496.45 | Részletek megtekintése |
![]() | ![]() | 13314 | TMP102 DIGITAL TEMP SENSOR BOARD | 254 - Immediate | $1,905.73 | Részletek megtekintése |
![]() | ![]() | LTL-4224 | LED RED CLEAR T-1 3/4 T/H | 73475 - Immediate | $44.84 | Részletek megtekintése |
![]() | ![]() | SC1633 | RASPBERRY PI PICO 2 W RP2350 | 6111 - Immediate | $2,242.03 | Részletek megtekintése |
![]() | ![]() | SC1634 | RASPBERRY PI PICO 2 WH RP2350 | 2388 - Immediate | $2,562.32 | Részletek megtekintése |
![]() | ![]() | SC1631 | RASPBERRY PI PICO 2 RP2350 | 26210 - Immediate | $1,601.45 | Részletek megtekintése |
![]() | ![]() | SC1632 | RASPBERRY PI PICO 2 H RP2350 | 1693 - Immediate | $1,921.74 | Részletek megtekintése |