The Surprising Innovations Steel Cable Ties Hold for Harsh Environments

Can the lowly cable tie be considered an engineering marvel? In my experience, yes—especially when it comes to steel cable ties. These ties are available with innovative features that can increase longevity beyond 30 years, even in the face of extreme temperatures, corrosive chemicals, strong vibration, or intense UV rays.

The locking mechanism is an important example. While steel bands are extremely durable, an improperly designed locking mechanism can slip due to factors such as heat expansion and liquid intrusion. Such slippage can be particularly problematic for hard-to-inspect locations that are common in refineries, ships, and other rough environments.

One way to avoid these issues is with a locking ball mechanism, like that illustrated in Figure 1. Once the cable tie is threaded through the head, the metal ball becomes wedged into the locking head, creating a tight grip that will not loosen over time. The features marked with asterisks are patented (*) by Panduit.

Figure 1: A locking-ball mechanism holds a steel cable tie in place by wedging into the locking head. (Image source: Panduit)

While all locking ball mechanisms use the same operating principle, some steel cable ties use unique designs that improve their performance. For example, the Pan-Steel MLTC Series from Panduit includes several patented and patent-pending features that simplify installation, increase locking strength, and improve bundle conformance.

Material selection

Of course, the stainless-steel bands are not immune to damage. Figure 2 lists some of the common options for metal cable ties and their suitability for various environments. Note that steel cable ties can be coated with nylon or polyester to make them more suitable for certain applications, such as contact with aluminum cable trays. However, these coatings come with downsides, such as lower tensile strength and greater vulnerability to environmental hazards.

Figure 2 : Shown are some of the environmental hazards to consider and the suitability of various materials to these conditions. (Image source: Panduit)

One of the most important factors to consider in material selection is temperature rating. When I started designing equipment for refineries, I was shocked at the extreme heat I encountered. Many areas of the plant had operating temperatures of several hundred degrees Celsius.

That’s why steel is such a great material for cable ties in extreme environmental conditions. As shown in Figure 3, the two common grades of steel can tolerate temperatures of -80°C (112°F) to 538°C (1,000°F). Coated steel cable ties have considerably narrower operating temperature ranges but are still suitable for many rugged applications like oil rigs, railways, or utility infrastructure.

Figure 3 : Stainless steel is rated for temperatures up to 1000° Fahrenheit, but when coatings are used, their temperature ratings must also be considered. All temperatures are in degrees Fahrenheit. (Image source: Panduit)

Worker safety and productivity

It’s also important to take workplace safety into consideration. I’ve had the misfortune of experiencing unsafe on-site conditions, so I have a first-hand appreciation of the hazards workers face.

To protect workers, I recommend choosing steel cable ties with rounded edges and a flush cutoff. These cable ties reduce the risk of laceration, which safeguards not only the technician but also the bottom line. The Occupational Safety and Health Administration (OSHA) estimates that a business can lose nearly $10,000 per laceration.

Also, take a moment to consider the effort required to install the cable ties. Equipping workers with the right tool not only leads to higher productivity, it can also reduce strain and injury. Some of the most common tools include:

  • Manual tensioning tools to tighten a cable tie until it reaches the desired tension
  • Automatic cutting tools to cut off the excess strap after the cable tie is tightened
  • Battery-powered tools to tension and cut stainless steel cable ties quickly and easily
  • Cable tie guns designed to tension and cut cable ties in one easy step

Figure 4 illustrates one popular option, the GTS-E cable-tie hand tool. This ergonomic tool is notable for its comfort, performance, and durability.

Figure 4 : The GTS-E cable-tie hand tool is designed for use with Pan-Steel MLTC Series cable ties. (Image source: Panduit)

Conclusion

Steel cable ties are often overlooked as simple fastening tools. In reality, they are critical to equipment longevity and worker safety in harsh environments, thanks to design features like locking mechanisms and rounded cable tie edges, as well as the development of ergonomic tooling. That’s why, when examined closely, steel cable ties are indeed marvels of engineering.

About this author

Image of Kenton Williston

Kenton Williston 2000-ben szerzett diplomát villamosmérnöki szakon, és pályafutását processzorok teljesítménymutatóinak vizsgálatával kezdte elemzőként. Ezután szerkesztőként dolgozott az EE Times csoportnál, és az elektronikai iparágon belül tevékenyen részt vett több kiadvány létrejöttében és konferenciák megszervezésében.

More posts by Kenton Williston
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum